This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3220: possibility of DC...100 Hz bandwith operation

Part Number: TPA3220


Hello, the datasheet states that the inputs "need to be AC coupled to minimize the output DC-offset and ensure correct ramping of the output voltages during power-ON and power-OFF".

Is that absolutely necessary or one could use the amplifier in PBTL mode for DC-100 Hz bandwidth as a closed loop operated coil driver. I need a power efficient output stage that could drive a pair of coils (Helmholtz configuration, something like 10 Ohms, 50 mH). The feedback would be “magnetic” and the TPA3220 driven by an output of op-amp integrator (ideally 0-5V signal, 2.5V meaning zero current...)

Thank you for any info