Part Number: LM4675
Hello,
I'm doing some emergency triage work on a a LM4675 design that is not passing EMI. It's used in a single-ended input:
IN+: has 51k ohm resistor + 0.1uF cap all in series to GND.
IN- has a 12.4k ohm resistor + 100uf Tantalum (yes, that's right) all in series from the source.
Source is CM119B CODEC, line level output. According to the datasheet, output voltage (rms) is 0.995 ohms into 10kOhm loading.
The output of the LM4675 is driving an 8ohm nominal impedance speaker. Each output (Vo1 and Vo2) has 1 100pF cap to GND plus 1 ESD diode to GND, then the connector for the speaker.
Decoupling power pins is (total) one 4.7uF cap, and two 0.1uF caps.
See attached.
I noticed that they've cut up the ground plane - I'm thinking that one change to make would be to use one continuous ground plane for the LM4675 and the CM119B CODEC, right?