Part Number: TLV320DAC32
Other Parts Discussed in Thread: CC8520,
I am trying to use the internal LDO in the TLV320DAC32 to power its core DVDD. I'm noticing the DVDD rail takes a very long time (several hundred milliseconds) to come up and I'm wondering whether this is typical. I'm using the DAC as a slave to a Purepath Wireless chipset (CC8520). The delay in turning on DVDD seems to be causing the DAC to not ACK any I2C commands from the CC8520, and once DVDD is up the DAC responds on I2C correctly.
Can TI offer any guidance on using the LDO? Do I have to wait several hundred msec for it to come up before writing, or is something going wrong in my design?
In below scope shots, yellow is DAC_RESETN, blue is AUD_I2C_SCL, green is AUD_I2C_SDA, and red is VDD at C653.
The first picture is a non acked I2C write while DVDD is low. The second picture is acked while DVDD is high. The last two pictures are wider timebase shots where we see DVDD turning on.