Other Parts Discussed in Thread: TPA711, TAS5630, TAS5615, TAS5613
Class AB amplifier efficiency in SE configuration
Q: Class AB amplifier efficiency in SE configuration
A customer wants to use a TPA711 in SE mode to drive a 15 Ohm speaker. Could you provide some design equations for calculating the efficiency of the audio amp and also the average current drawn so that i can calculate the amplifier dissipation. There is a detailed calculation for BTL in the datasheets.
A: Re: Class AB amplifier efficiency in SE configuration
The equations for efficiency for BTL and SE are the same except for the IDDrms calculation. For SE, IDDrms = Vp/(pi*RL) or half the value for BTL. This will make the amplifier twice as efficient as BTL for the same output power. Keep in mind these equations are only valid for sine waves and they assume the user has gotten rid of the DC current that will be flowing in single ended configuration. This can be done by using a DC blocking cap or tying the other end of the speaker to Vdd/2 instead of ground.
If this DC current is not removed, then an additional power dissipation of Vdd^2/RL will be occur, which will cause a drop in the efficiency of the system.
Consumer Devices in Industrial Applications
Q: TAS5630 ambient temp
Hello,
I would like to use the TAS5630 for an industrial application.
What will happe if i use it in an environment with an ambiante tempeature higher than 70°C (Reduce the MTBF, malfunction, reduce the performance?)
Is it expected in the future an industrial range for this type of component?
Thanks
A: Re: TAS5630 ambient temp
Officially, the manufacturer (TI) does not guarantee ANY device specs or even device operation outside of the noted operating temperature range.
However, many consumer devices will operate just fine under typical 'industrial' ambient operating conditions. Specs that typically change at high temperatures include increased noise and worse power vs. thd performance. Also, the device may go into thermal protection when outputting "normal" power levels. For abnormal operating conditions it is best to test the specs that are important to your system at the extreme conditions.
One point that is hard to test, but is a very legitimate concern is long term device operation. If a device is consistently operated outside of the specified conditions, long term reliability may suffer (i.e. the device may fail well before the expected lifetime is up). Again, this goes back to the point that the manufacturer does not guarantee operation outside of the specified range.
Finding a device's weight (mass)
All devices released to production and orderable on ti.com will have this info. Please look in the device's product folder on ti.com.
- Go to Quality & Environmental Data
- Select View under Details column for the device
- Scroll to the right under Package Details
- Look for Device Mass.
General Suggestions on TDMA Noise in portable products
Guideline for fixing heat sink on PHD, DKD, and DDV packages
Guideline for fixing heat sink
Q: Do you have any spec or guideline for max torque for fixing heat sink on TAS5615/5630PHD?
A: There is no easy answer to this question as it depends on several system-level variables.
In general, we recommend using a thin layer of non-conductive, thermally-conductive heat sink grease. The layer should be extremely thin, the goal is to fill any tiny gaps between the device pad and the heat sink. The thermal conductance of the heat sink grease is >> metal to metal contact, so try to limit the thickness of the heat sink grease used to maximize the thermal performance of your system.
Secondly, be careful that you do not warp your board, especially when using one heat sink for multiple devices. You want to torque the screws in an order that does not cause board warping. If there is board warping due to poor sequence or uneven torquing of the screws, you will hurt the thermal performance of your system.
We also recommend tapping the heat sink and using machine screws to connect it. If you use self-tapping screws, you run the risk of introducing shards of metal in your system which could result in a short in your system.
Finally, be careful with your stencil thickness and stand-off height. Ideally, you don't want to stress the pins as they enter the package as this could result in broken pins over the lifetime of your product.
The max loads are
PHD and DDV - max load is 90 Newtons
DKD - max load is 200 Newtons
Measuring the impedance of a loudspeaker
Surfing thru the forum, you'll see many threads related to short-circuit protection and over-current protection problems. These are usually caused by one of two things: 1) a poor output filter design, or 2) an unknown dip in speaker impedance.
For #2, if you use a DMM to measure the speaker impedance, you only get part of the picture - DC. Since a speaker is comprised of a complex impedance, you really need to measure it across frequency.
Automatic Loudspeaker Equalizer Software
Need a .bxl file generated?
A .bxl file is a "Binary XLator" file which is intended to be a universal footprint for any layout program. ADI has an app note which describes it.
Usually, these are stored in the Product Folder in the web under the "Quality & packaging" tab and then "CAD/CAE symbols."
If the file is not posted there, you will need to request a new one be generated (please make sure it then gets posted to the Product Folder for other customers!):
Submit a model request at http://webenchmodeling/ModelRequestSurvey.aspx. Select the Altium symbol/footprint category, and in the Comments section state that this is a .bxl request.
Quick Reference guide to Max output power of a Class D amplifier
Q: Quick Reference guide to Max output power of a Class D amplifier
A: Re: TAS5613 - max output power from 24V to 4ohm load?
Hi,
The pdf file attached at the end of this post shows how to approximate the max output power for a Class D at a given PVDD and load. It uses the TAS5613 as an example with PVDD = 24V and a 4 ohm load.
What the file shows is that the RDSON of the device creates a voltage divider with the load. It shows that the largest unclipped sine wave will have about 65W and a clipped signal (10% THD) will be 81.6. Note that the calculation of 10% THD is an approximation that says P_clipped = 1.25* P_unclipped.
If RdsOn were 0 ohm resistance (ideal output stage), the power would be 72W unclipped and 90W clipped.
Replacing NXP "End of Life" audio amps with TI devices
Replacing NXP "End of Life" audio amps with TI devices
We've been noticing a lot of requests for similar parts to replace the NXP devices that are being discontinued. I've made a comprehensive list for these NXP devices and their TI replacements below. Note: they are not pin-to-pin replacements; they are the most similar parts based off of architecture and output power.
|
NXP Part# |
Most Similar TI Part |
What is BTL configuration?
| Problem: What is BTL configuration? How is BTL different than SE?
|
| Solution: BTL is an acronym for "bridge-tied load." A bridge-tied load configuration consists of one amplifier driving one side of a load and another amplifier (with an inverted signal from the first amplifier) driving the other side of the load. This results in 2x more voltage swing across the load than you would have in a single-ended configuration where one side of the load is tied to an amplifier and the other side to ground. Twice the voltage swing across the load equates to 4x the power to the load (P = V^2/R). So, a BTL load configuration offers 4x more power to the load than a single ended configuration from the same supply voltage. Be aware, that BTL amplifiers dissipate 4x the heat of a Single-Ended amplfier under the same supply voltage and load conditions. Refer to the TPA7x1 series parts in the applications section for more on BTL. Also note that the output DC blocking capacitors are NOT required in the BTL configuration. Since the load is tied across two amplifiers with the same DC bias and the signal across the load is the difference between the amplifier outputs, the DC bias is removed. |