Other Parts Discussed in Thread: PCM9211
Hello,
I am currently designing and programming the TAS3251.
However, I still have some problems with the DAC output. Currently, sounds above 1.5kHz are distorted, because the smoothed signal looks very modest after the DAC. I actually followed the design of the Eval Board 1:1, but I am currently not sure if the documentation of the Eval Board is the same as the actual assembly of the Eval Board. Is the circuit diagram of the Eval Board correct at this point?
Or can/must I adjust the frequency of the DAC?
With kind regards,
Simon