Hi,
I've made an attempt at an audio circuit using the TPA3110D2, however I'm having issues with the output. I've made a few modifications compared to the reference design on the datasheet, like adding transformers between the input and the chip, and there seems to be no issues with that part. However, there is no audio signal coming out, I've measured the output at the terminals and it seems to show a DC voltage (around 5V). I'm probably missing something obvious but I can't seem to figure it out. I've included an image of the audio circuit schematic.