Other Parts Discussed in Thread: DIR9001, , TAS6422Q1EVM
I have built a circuit using TAS6422 and DIR9001 using the TAS6422Q1-EVM as a reference design. I get no sound and only 44ma of current. PVDD and VBAT are tied together receiving 14.4V. VDD is receiving 3.3V. I2S from DIR9001 to TAS6422. Followed reference design to a T. There is no heatsink attached, but the thermal pad is internally connected to gnd and I have personally connected it to ground with jumper wire and it makes no difference.
The WARN pin asserts itself immediately. On the scope, current spikes at about 2A, WARN pin asserts, as 14.4 V just beings to ramp up. 14.4V ramps up in about 15ms. I try talking to it through i2c using the PPC3 gui but it will not come up to connect.
I really need help on this. I am trying to build the audio amplifier for my company and we would like to use it in our design.
Thank you for your time.