Part Number: SRC4382
In order to keep the integrity of the digital inputs, could you please forward the signals coming from the DIR inputs and Port A I2S directly to Port B without passing through the ASRC.How to configure the software?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SRC4382
In order to keep the integrity of the digital inputs, could you please forward the signals coming from the DIR inputs and Port A I2S directly to Port B without passing through the ASRC.How to configure the software?
Dear Ravi
Thanks!
Also, for the S/PDIF signal from the DIR input, can it be output directly from the PORTB port without going through the ASRC?
The input from the PORTA port is the I2S signal, and the output from the PORTB port is also I2S. In this case, the input and output signal formats are the same.
But the input from the DIR is the S/PDIF signal, and the output from the PORTB port is I2S. In this case, the input and output signal formats are different.