Part Number: TLV320ADC3001
I am using the TLV320ADC3001 with a mono single ended ac coupled source connected to IN1L(P). I have it configured to I2S 24 bit mode. With no input signal the voltage at IN1L(P) is around 1.35V as I would expect. However, the data values I see are around 0x01700, not hovering around zero as I would expect. It feels like the ADC is giving me the dc voltage at the input.