Tool/software: Linux
hello.
I using wm8731 audio codec witch is connected to CORE9x35 module with SSC and I2C0 interface (linux: linux-at91-linux4sam_5.5), it works about 95%, 5% I2C0 goes in timeout and when i check, SDA pin pulled low from WM8731 chip, after this I must switch power of and on again if I want sound or I must pull down SCL pin and release again then SDA pin goes too high (released) PLEASE HELP,I think it is same issue :