This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2912 Linux Driver

Part Number: PCM2912


Tool/software: Linux

Dear,

Our ctm want to use PCM2912; and the software environment is linux.

Could we can provide this device drive in linux system? Thanks!

Best regards

  • Hi, Sundy,

    The PCM2912A is a USB-audio codec which uses the native USB Audio Class driver from the host Operating System. There is no need for an extra driver to operate with Linux systems as the UAC driver should be part of the OS. 

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer