Dear Sirs,
My customer asked us about TDM mode for PCM1864.
He is planning to use it with 4ch ADC. In that case, he thinks that PCM1864 can only select TDM as the data transfer method.
However, he thinks the content is compatible with the TDM format of the PCM1864 and the customer's microcomputer side.
The microcomputer side only supports the mode that sets only the first 1 word to H.
If PCM 1864 is used under this condition (In the mode to set only the first 1 bit to H and input the following SSIWS to LRCK), will it still operate normally?
Please let us know above question.
Best Regards,
Y.Hasebe