Part Number: LM4666
Other Parts Discussed in Thread: TPA2006D1, TPA2005D1, TPA2012D2
Hi Team,
One of my customers wants to use LM4666 as amplifier for 1W 8 ohm speakers( 2 in No.)
The input is analog coming from SOC which supports 100-200mW for speaker.
Following are the queries:
-
The output power of LM4666 is 1.2W @5V supply. We are planning to connect 2 nos 1W, 8ohm speaker. Whether LM4666 will support the same.
2. Input voltage range for analog input pin is not mentioned in LM4666 datasheet(Only absolute maximum information is there). Please share the same.
Regards,
Harmeet