This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5411-Q1: question about Load Diagnostics duration time variation

Part Number: TAS5411-Q1


Hello Experts,

My customer wants to know duration time of DC load diagnostics, and so on. Would you please answer to below question?
1. Load Diagnostics is always run if it deasserted from standby mode, correct?
2. If so, load diagnostics can be disabled by I2C? My understanding is it can not.
3. According to datasheet, load diagnostics duration time is 229ms. Does it have some variation? If so, please tell the approximately number.
4. After finish the load diagnostics tests, how much time is needed to start the audio output? I think it is needed bit long time due to reducing pop-noise.

Your support would be much appreciated.
Best Regards,
Fujiwara