Part Number: PCM5242
Hello,
I have a pcm5242rhbevm. It was working fine with the purpath console. It was reading "Audio EVM" in the device manager of windows. I then did some testing on the i2c, and then tried to go back to using the pureoath console. After going back, the device is not shown as an "Unknown Device" in windows device manager. I tried uninstalling the entire thing and rebooting and reinstalling. That didn't change anything. I tried installing into a new pc. That didn't change anything. Now concerned that the USB chip found on the EVM is no longer programmed and therefore the device is bricked without getting the firmware reflashed.
Can you tell me if there is anything else I should try? I know the jumpers are in the same position they used to be in when working fine with the purpath console
But now after some toying around it will not recognize.
Any advice? I'd rather not buy another evm... Thanks for your help.
Jay