Hi,
I am using the TLV320AIC3204 codec in an application where I need to accurately detect the time of arrival of an audio signal. At 44.1 kHz sampling rate I seem to get a 0.5ms delay from starting to transmit the data to the audio signal appearing on the line out and a 0.5ms delay at the ADC (audio signal arriving at the MIC to available at McBSP receive register). At 32kHz sampling rate I get a 2ms delay from starting to transmit the data to the audio signal appearing on the line out and a 1.5ms delay at the ADC.
Can anyone tell me what exact delay I should expect to get? I expect that it should be related to the sampling rate, oversampling rate and maybe which signal processing clocks are enabled (I've got DOSR=128 and AOSR=128, PTM_R4, PRB_P1 and PRB_R1).
regards,
Charles