Tool/software: TI C/C++ Compiler
Dear Sir:
could you help check if have LM49352 reference driver code , Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Dear Sir:
could you help check if have LM49352 reference driver code , Thanks
Dear Steve:
Thanks for youe reply , the problem of our customer is the LM49352 can not run, and could you help check if the register is set correct .
lm49352_write=> reg:0x00=0x00b
lm49352_write=> reg:0x01=0x001
lm49352_write=> reg:0x03=0x001
lm49352_write=> reg:0x11=0x002
lm49352_write=> reg:0x12=0x001
lm49352_write=> reg:0x1b=0x000
lm49352_write=> reg:0x20=0x033
lm49352_write=> reg:0x21=0x00b
lm49352_write=> reg:0x30=0x031
lm49352_write=> reg:0x44=0x009
lm49352_write=> reg:0x50=0x007
lm49352_write=> reg:0x04=0x000
lm49352_write=> reg:0x05=0x0ec
lm49352_write=> reg:0x06=0x014
lm49352_write=> reg:0x07=0x00d
lm49352_write=> reg:0x10=0x003
lm49352_write=> reg:0x13=0x023
lm49352_write=> reg:0x18=0x02b
lm49352_write=> reg:0x23=0x00f
lm49352_write=> reg:0x42=0x005
lm49352_write=> reg:0x80=0x004
lm49352_write=> reg:0x84=0x00a
lm49352_write=> reg:0x85=0x00a
lm49352_write=> reg:0x86=0x00a
lm49352_write=> reg:0x87=0x01f
lm49352_write=> reg:0x89=0x033
lm49352_write=> reg:0x8a=0x033
lm49352_write=> reg:0xa0=0x002
lm49352_write=> reg:0xa3=0x00a
lm49352_write=> reg:0xa4=0x00a
lm49352_write=> reg:0xa5=0x00a
lm49352_write=> reg:0xa6=0x033
lm49352_write=> reg:0xa8=0x033
lm49352_write=> reg:0xa9=0x033
lm49352_write=> reg:0x16=0x00f
lm49352_write=> reg:0x15=0x00c
lm49352_read <= reg:0x02=0x1ff