Other Parts Discussed in Thread: TAS5751M
Hi,
I am using PUREPATH-CMBEVM with our TAS5751M PCB design. All the I2C and I2S from PUREPATH-CMBEVM are linked to the other board.
During the hardware check in Console, the Hardware ID is incorrect. I checked the I2C signals sent through the Console attached below.
based on the datasheet pg 24, The 7-bit address for the TAS5751M device is 0101 010 (0x54) or 0101 011 (0x56) as defined by ADR/FAULT
(external pulldown for 0x54 and pullup for 0x56). However; the fig below shows that PUREPATH-CMBEVM is sending 1010 100 which is actually revers of (0x56) . what can be the reason??