Is it allowed to supply power only to DVDD, and not to apply to AVDD and PVDD ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it allowed to supply power only to DVDD, and not to apply to AVDD and PVDD ?
My device can be powered through а USB connector аs well аs from an external power source. In case of power being provided through the USB, it's necessary to prevent sound generation on hardware level. For that purpose TAS5720A-Q1 IC should be (if that is possible) suplied only through DVDD line. In the case of external power source, TAS5720A-Q1 IC will be supplied through all the necessary lines.
Not exactly. What I actually want to do is to block any possibility to generate sounds (intentional or not) when device is powered through the USB.