Part Number: PCM1861
Other Parts Discussed in Thread: PCM5100A
Dear Sir,
Would you please help give a suggestion about below requirement?
It is a 2 I2S source, with one stereo DAC. Maybe can use a digital switch + DAC to reach the target.
I2S1: BCLK, WCLK, DATA
I2S2: BLCK, WCLK, DATA
The DAC performance are as below:
1. I2C control, HW control is better
2. (first) Built-in PLL or (second) asynchronized external clock
3. Support 16bit I2S data
4. THD+N > 80dB
5. Vo(full scale) > 0.9Vrms
6. Single-end output is ok
7. Power source = 3.3V is better
8. Temp -20~+85
Thanks, Ian.