I am a new-B when it comes to audio, so this might be a silly question. I am putting together a very thin audio recording/playback device that must be no taller than 1/8", and this project requires a very thin speaker. I ordered a APS2718S-T-R piezo speaker from PUI Audio Inc. for no particular reason other than DigiKey had them in stock, it looks cool, and it's REALLY thin. I want to glue the piezo speaker to a TLV320AIC3120 because I'm pretty sure I will need the filtering capabilities, and I want to justify my purchase of the EVM board that just showed up in the mail. The TLV part has a class D 8-ohm speaker output. I understand I cannot connect the piezo speaker to the TLV part because the impedance and voltage levels are all wrong, so I was going to use the line output from the TLV part and feed that to a TPA2100 class D piezo driver chip and not use the speaker driver output from the TLV device. I'm wondering if it would be any better to use a transformer instead and drive the piezo speaker using the speaker driver on the TLV part through the transformer and save battery power by dumping the piezo driver chip. Is that dumb? If I have a step-up transformer made with a primary impedance of 8-ohms and a secondary impedance of 300 (the impedance of the piezo) with about a 5:1 turns ratio, can that eliminate the TPA2100 driver chip? Any better suggestions?
Thanks!
Dave