This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: Asking for ADC3101 input source format

Part Number: TLV320ADC3101

Hi team,

Customer uses ADC3101 on the IBI8 platform.

Here is the MCLK, BCLK, WCLK and DOUT waveform.

Would you please review the waveform to see any abnormal?

BR,

SHH

  • Hi, SHH,

    The waveform shared actually seems to be in TDM/DSP format, not I²S, so the parameters of the table you are sharing are not applicable; please look to table 8.10. The waveform seems fine, but the only thing which should be double-checked is the ADC Data out, which seems to have an offset of half bit clock cycle, which may be a result of the Bit clock polarity used. Please review Page 0: Register 2 and let me know if you see any change in the output after changing the value of bit D3.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • Hi Diego,
    P0R2 D3 definitions seem not show in the datasheet.
    Could you please provide this register setting for us?

    BR,
    SHH
  • Hi, Shh,

    Page 0: Register 2 is reserved, but I see the issue, there is a typo on my response, where the correct register to change the polarity of the bit clock is Page 0: Register 29.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer