This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA4311: PGA4311 - output impedance.

Part Number: PGA4311


Hello everybody,

I have a question about PGA4311. What is the output impedance of this chip? I want to connect the output with the input to realize two-stage volume control (pre volume and master volume). I read in datasheet then: "For optimal performance, it is best to drive the PGA4311 with a low source impedance. A source impedance of 600Ω or less is recommended."

Thanks for any help.