This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to choose the proper OPAs in TI website?

Other Parts Discussed in Thread: OPA1678, OPA1679, OPA1642, OPA1692, OPA1662, OPA1622, OPA1688, INA1620

Hi,

So many OPA chipsets in TI websits , how could i know which is better and suit for my application because of little difference between them,  do you have some suggestions on audio amplifiers ? for example , some roadmap on audio amplifier , or the comparaion between these OPAs.

My application scenarios is below:

1. MIC amplifier

2. Microphone Amplifier

Thanks and Regards

William

  • Hi William,
    We have published an audio selection guide (www.ti.com/.../slot140.pdf) which gives a comparison of many of our audio devices.

    As far as which amplifier to select for a given application, that's going to depend a lot on what specifications you're targeting. A bipolar input op amp will have lower voltage noise, but its higher current noise is problematic when working with high-impedance inputs. FET and CMOS input op amps have higher voltage noise than bipolar amplifiers, but have very low current noise, which often makes them a better choice when interfacing with high impedance sources.

    Other concerns would be cost, power consumption, especially in battery powered applications, and more.

    A few good building-block audio op amps:
    OPA1678/OPA1679 - FET input, low cost, good performance. Good noise performance (4.5nV/rtHz at 1kHz).
    OPA1642 - FET input, lower distortion than OPA1678, but higher cost. Higher broadband noise (5.1nV/rtHz at 1kHz) than OPA1678, but lower 1/f noise
    OPA1692 - Bipolar input, very low power (650µA/channel)
    OPA1662 - bipolar input, low power.

    For higher output power applications, like headphone drive:
    OPA1622 - bipolar
    OPA1688 - FET
    INA1620 - bipolar
  • Hi, Alex

    Thanks a lot for your quick response. it is very helpful for me.

    William