Hi
At the beginning of the data sheet this device is advertised as being able to sample up to 96kHz. However reading further it is not clear if the actual available bandwidth is limited to just below 20kHz.
We chose this device because of the 96kHz advertised sampling rate.
Can you let us know if we were to set the device to 96kHz sampling if we would get a real usable bandwidth of just below 48kHz (both for the ADC and the DAC) or if the bandwidth is limited to 20kHz but over sampled at 96kHz?
Thanks
Manjula