Other Parts Discussed in Thread: LF442QML,
Hello,
I have been using LF442QML (actual orderable part number is LF442MH/883 N) which I believe was tested to Mil-Std-883, Method 5005 - Group A. Now I see this product is no longer offered. However I can purchase LF442AMH which states -55 to 125degC operation. Can you tell me the actual differences of the two parts? Note I only can find the data sheet for the LF442QML from external content aggregators.
Also If the LF442AMH is not tested to the '883 standard above then can you tell me if this is still using the same package materials or have there been other changes?
Thank you,
HSG