Other Parts Discussed in Thread: CC3200AUDBOOST
We are using the CC3200AUDBOOST for a audio over RF project and have some questions:
-Could you confirm that the range of J is according to this post:
The post is 3 years old and the documentation is not updated. If J have to be larger than 4, what happens if set to lower?
- What happens if equation (20) on page 78 in
is not true?
- I tried the GUI to calculate the PLL numbers but it looks like it require a EM plugged in. Do we have a tool that work without any hardware connected?