Other Parts Discussed in Thread: TAS5782M
Tool/software: Linux
Would you please share us the Linux drive or programming guide of TAS5751?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Billy,
Unfortunately we don't have the Linux driver for TAS5751M. You could generate the register configuration head file by TAS5751M EVM and PPC3 GUI. Please find more detailed info in the TAS5751M EVM user's guide:
Then you could write the driver with it. Here is an example for another product TAS5782M, hope it helps you.
/* * Driver for the TAS5782M Audio Amplifier * * Author: Andy Liu <andy-liu@ti.com> * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License * version 2 as published by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, but * WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * General Public License for more details. */ #include <linux/module.h> #include <linux/moduleparam.h> #include <linux/slab.h> #include <linux/of.h> #include <linux/init.h> #include <linux/i2c.h> #include <linux/regmap.h> #include <sound/soc.h> #include <sound/pcm.h> #include <sound/initval.h> #include "ppc3_tuning_-30dB.h" #define TAS5872M_DRV_NAME "tas5782m" #define TAS5872M_RATES (SNDRV_PCM_RATE_48000) #define TAS5782M_FORMATS (SNDRV_PCM_FMTBIT_S16_LE | SNDRV_PCM_FMTBIT_S20_3LE |\ SNDRV_PCM_FMTBIT_S24_LE | SNDRV_PCM_FMTBIT_S32_LE) #define TAS5782M_REG_00 (0x00) #define TAS5782M_REG_03 (0x03) #define TAS5782M_REG_7F (0x7F) #define TAS5782M_REG_14 (0x14) #define TAS5782M_REG_15 (0x15) #define TAS5782M_REG_16 (0x16) #define TAS5782M_REG_17 (0x17) #define TAS5782M_REG_44 (0x44) #define TAS5782M_REG_45 (0x45) #define TAS5782M_REG_46 (0x46) #define TAS5782M_REG_47 (0x47) #define TAS5782M_REG_48 (0x48) #define TAS5782M_REG_49 (0x49) #define TAS5782M_REG_4A (0x4A) #define TAS5782M_REG_4B (0x4B) #define TAS5782M_PAGE_00 (0x00) #define TAS5782M_PAGE_8C (0x8C) #define TAS5782M_PAGE_1E (0x1E) #define TAS5782M_PAGE_23 (0x23) const uint32_t tas5782m_volume[] = { 0x07ECA9CD, //24dB 0x07100C4D, //23dB 0x064B6CAE, //22dB 0x059C2F02, //21dB 0x05000000, //20dB 0x0474CD1B, //19dB 0x03F8BD7A, //18dB 0x038A2BAD, //17dB 0x0327A01A, //16dB 0x02CFCC01, //15dB 0x02818508, //14dB 0x023BC148, //13dB 0x01FD93C2, //12dB 0x01C62940, //11dB 0x0194C584, //10dB 0x0168C0C6, //9dB 0x0141857F, //8dB 0x011E8E6A, //7dB 0x00FF64C1, //6dB 0x00E39EA9, //5dB 0x00CADDC8, //4dB 0x00B4CE08, //3dB 0x00A12478, //2dB 0x008F9E4D, //1dB 0x00800000, //0dB 0x00721483, //-1dB 0x0065AC8C, //-2dB 0x005A9DF8, //-3dB 0x0050C336, //-4dB 0x0047FACD, //-5dB 0x004026E7, //-6dB 0x00392CEE, //-7dB 0x0032F52D, //-8dB 0x002D6A86, //-9dB 0x00287A27, //-10dB 0x00241347, //-11dB 0x002026F3, //-12dB 0x001CA7D7, //-13dB 0x00198A13, //-14dB 0x0016C311, //-15dB 0x00144961, //-16dB 0x0012149A, //-17dB 0x00101D3F, //-18dB 0x000E5CA1, //-19dB 0x000CCCCD, //-20dB 0x000B6873, //-21dB 0x000A2ADB, //-22dB 0x00090FCC, //-23dB 0x00081385, //-24dB 0x000732AE, //-25dB 0x00066A4A, //-26dB 0x0005B7B1, //-27dB 0x00051884, //-28dB 0x00048AA7, //-29dB 0x00040C37, //-30dB 0x00039B87, //-31dB 0x00033718, //-32dB 0x0002DD96, //-33dB 0x00028DCF, //-34dB 0x000246B5, //-35dB 0x00020756, //-36dB 0x0001CEDC, //-37dB 0x00019C86, //-38dB 0x00016FAA, //-39dB 0x000147AE, //-40dB 0x0001240C, //-41dB 0x00010449, //-42dB 0x0000E7FB, //-43dB 0x0000CEC1, //-44dB 0x0000B845, //-45dB 0x0000A43B, //-46dB 0x0000925F, //-47dB 0x00008274, //-48dB 0x00007444, //-49dB 0x0000679F, //-50dB 0x00005C5A, //-51dB 0x0000524F, //-52dB 0x0000495C, //-53dB 0x00004161, //-54dB 0x00003A45, //-55dB 0x000033EF, //-56dB 0x00002E49, //-57dB 0x00002941, //-58dB 0x000024C4, //-59dB 0x000020C5, //-60dB 0x00001D34, //-61dB 0x00001A07, //-62dB 0x00001733, //-63dB 0x000014AD, //-64dB 0x0000126D, //-65dB 0x0000106C, //-66dB 0x00000EA3, //-67dB 0x00000D0C, //-68dB 0x00000BA0, //-69dB 0x00000A5D, //-70dB 0x0000093C, //-71dB 0x0000083B, //-72dB 0x00000756, //-73dB 0x0000068A, //-74dB 0x000005D4, //-75dB 0x00000532, //-76dB 0x000004A1, //-77dB 0x00000420, //-78dB 0x000003AD, //-79dB 0x00000347, //-80dB 0x000002EC, //-81dB 0x0000029A, //-82dB 0x00000252, //-83dB 0x00000211, //-84dB 0x000001D8, //-85dB 0x000001A4, //-86dB 0x00000177, //-87dB 0x0000014E, //-88dB 0x0000012A, //-89dB 0x00000109, //-90dB 0x000000EC, //-91dB 0x000000D3, //-92dB 0x000000BC, //-93dB 0x000000A7, //-94dB 0x00000095, //-95dB 0x00000085, //-96dB 0x00000076, //-97dB 0x0000006A, //-98dB 0x0000005E, //-99dB 0x00000054, //-100dB 0x0000004B, //-101dB 0x00000043, //-102dB 0x0000003B, //-103dB 0x00000035, //-104dB 0x0000002F, //-105dB 0x0000002A, //-106dB 0x00000025, //-107dB 0x00000021, //-108dB 0x0000001E, //-109dB 0x0000001B, //-110dB }; struct tas5782m_priv { struct regmap *regmap; int volume_db; }; const struct regmap_config tas5782m_regmap = { .reg_bits = 8, .val_bits = 8, .cache_type = REGCACHE_RBTREE, }; static int tas5782m_vol_info(struct snd_kcontrol *kcontrol, struct snd_ctl_elem_info *uinfo) { uinfo->type = SNDRV_CTL_ELEM_TYPE_INTEGER; uinfo->access = SNDRV_CTL_ELEM_ACCESS_TLV_READ | SNDRV_CTL_ELEM_ACCESS_READWRITE; uinfo->count = 1; uinfo->value.integer.min = -110; uinfo->value.integer.max = 24; uinfo->value.integer.step = 1; return 0; } static inline int get_db(int index) { //input : 0 -- 134 //output : 24 -- -110 return (24 - index); } static int tas5782m_vol_get(struct snd_kcontrol *kcontrol, struct snd_ctl_elem_value *ucontrol) { struct snd_soc_codec *codec = snd_soc_kcontrol_codec(kcontrol); struct tas5782m_priv *tas5782m = snd_soc_codec_get_drvdata(codec); ucontrol->value.integer.value[0] = tas5782m->volume_db; return 0; } static inline unsigned int get_volume_index(int vol) { //input : 24 -- -110 //output : 0 -- 134 return (24 - vol); } static void tas5782m_set_volume(struct snd_soc_codec *codec, int db) { unsigned int index; uint32_t volume_hex; uint8_t byte4; uint8_t byte3; uint8_t byte2; uint8_t byte1; index = get_volume_index(db); volume_hex = tas5782m_volume[index]; byte4 = ((volume_hex >> 24) & 0xFF); byte3 = ((volume_hex >> 16) & 0xFF); byte2 = ((volume_hex >> 8) & 0xFF); byte1 = ((volume_hex >> 0) & 0xFF); #if 1 //w 90 00 00 snd_soc_write(codec, TAS5782M_REG_00, TAS5782M_PAGE_00); //w 90 7f 8c snd_soc_write(codec, TAS5782M_REG_7F, TAS5782M_PAGE_8C); //w 90 00 1e snd_soc_write(codec, TAS5782M_REG_00, TAS5782M_PAGE_1E); //w 90 44 xx xx xx xx snd_soc_write(codec, TAS5782M_REG_44, byte4); snd_soc_write(codec, TAS5782M_REG_45, byte3); snd_soc_write(codec, TAS5782M_REG_46, byte2); snd_soc_write(codec, TAS5782M_REG_47, byte1); //w 90 00 00 snd_soc_write(codec, TAS5782M_REG_00, TAS5782M_PAGE_00); //w 90 7f 8c snd_soc_write(codec, TAS5782M_REG_7F, TAS5782M_PAGE_8C); //w 90 00 1e snd_soc_write(codec, TAS5782M_REG_00, TAS5782M_PAGE_1E); //w 90 48 xx xx xx xx snd_soc_write(codec, TAS5782M_REG_48, byte4); snd_soc_write(codec, TAS5782M_REG_49, byte3); snd_soc_write(codec, TAS5782M_REG_4A, byte2); snd_soc_write(codec, TAS5782M_REG_4B, byte1); //w 90 00 00 snd_soc_write(codec, TAS5782M_REG_00, TAS5782M_PAGE_00); //w 90 7f 8c snd_soc_write(codec, TAS5782M_REG_7F, TAS5782M_PAGE_8C); //w 90 00 23 snd_soc_write(codec, TAS5782M_REG_00, TAS5782M_PAGE_23); //w 90 14 00 00 00 01 snd_soc_write(codec, TAS5782M_REG_14, 0x00); snd_soc_write(codec, TAS5782M_REG_15, 0x00); snd_soc_write(codec, TAS5782M_REG_16, 0x00); snd_soc_write(codec, TAS5782M_REG_17, 0x01); #endif } static int tas5782m_vol_put(struct snd_kcontrol *kcontrol, struct snd_ctl_elem_value *ucontrol) { struct snd_soc_codec *codec = snd_soc_kcontrol_codec(kcontrol); struct tas5782m_priv *tas5782m = snd_soc_codec_get_drvdata(codec); int db; db = ucontrol->value.integer.value[0]; tas5782m->volume_db = db; tas5782m_set_volume(codec, db); return 0; } static const struct snd_kcontrol_new tas5782m_vol_control = { .iface = SNDRV_CTL_ELEM_IFACE_MIXER, .name = "TAS5782M Software Volume", .info = tas5782m_vol_info, .get = tas5782m_vol_get, .put = tas5782m_vol_put, }; static int tas5782m_snd_probe(struct snd_soc_codec *codec) { int ret; ret = snd_soc_add_codec_controls(codec, &tas5782m_vol_control, 1); return ret; } static struct snd_soc_codec_driver soc_codec_tas5782m = { .probe = tas5782m_snd_probe, }; static int tas5782m_mute(struct snd_soc_dai *dai, int mute) { u8 reg3_value = 0; struct snd_soc_codec *codec = dai->codec; if (mute) reg3_value = 0x11; snd_soc_write(codec, TAS5782M_REG_00, 0x00); snd_soc_write(codec, TAS5782M_REG_7F, 0x00); snd_soc_write(codec, TAS5782M_REG_03, reg3_value); return 0; } static const struct snd_soc_dai_ops tas5782m_dai_ops = { .digital_mute = tas5782m_mute, }; static struct snd_soc_dai_driver tas5782m_dai = { .name = "tas5782m-amplifier", .playback = { .stream_name = "Playback", .channels_min = 2, .channels_max = 2, .rates = TAS5872M_RATES, .formats = TAS5782M_FORMATS, }, .ops = &tas5782m_dai_ops, }; static int tas5782m_probe(struct device *dev, struct regmap *regmap) { struct tas5782m_priv *tas5782m; int ret; tas5782m = devm_kzalloc(dev, sizeof(struct tas5782m_priv), GFP_KERNEL); if (!tas5782m) return -ENOMEM; dev_set_drvdata(dev, tas5782m); tas5782m->regmap = regmap; tas5782m->volume_db = -30; ret = regmap_register_patch(regmap, tas5782m_init_sequence, ARRAY_SIZE(tas5782m_init_sequence)); if (ret != 0) { dev_err(dev, "Failed to initialize TAS5782M: %d\n",ret); goto err; } ret = snd_soc_register_codec(dev, &soc_codec_tas5782m, &tas5782m_dai, 1); if (ret != 0) { dev_err(dev, "Failed to register CODEC: %d\n", ret); goto err; } return 0; err: return ret; } static int tas5782m_i2c_probe(struct i2c_client *i2c, const struct i2c_device_id *id) { struct regmap *regmap; struct regmap_config config = tas5782m_regmap; regmap = devm_regmap_init_i2c(i2c, &config); if (IS_ERR(regmap)) return PTR_ERR(regmap); return tas5782m_probe(&i2c->dev, regmap); } static int tas5782m_remove(struct device *dev) { snd_soc_unregister_codec(dev); return 0; } static int tas5782m_i2c_remove(struct i2c_client *i2c) { tas5782m_remove(&i2c->dev); return 0; } static const struct i2c_device_id tas5782m_i2c_id[] = { { "tas5782m", }, { } }; MODULE_DEVICE_TABLE(i2c, tas5782m_i2c_id); #ifdef CONFIG_OF static const struct of_device_id tas5782m_of_match[] = { { .compatible = "ti,tas5782m", }, { } }; MODULE_DEVICE_TABLE(of, tas5782m_of_match); #endif static struct i2c_driver tas5782m_i2c_driver = { .probe = tas5782m_i2c_probe, .remove = tas5782m_i2c_remove, .id_table = tas5782m_i2c_id, .driver = { .name = TAS5872M_DRV_NAME, .of_match_table = tas5782m_of_match, }, }; module_i2c_driver(tas5782m_i2c_driver); MODULE_AUTHOR("Andy Liu <andy-liu@ti.com>"); MODULE_DESCRIPTION("TAS5782M Audio Amplifier Driver"); MODULE_LICENSE("GPL");
Best regards,
Shawn Zheng