Hello!
We use the 3204 chip on the C5517 evaluation board with a project. Please help us solve the following problems.
1. What is the 3204 CM (Figure 1), please briefly introduce it?
2. We used an external microphone as the audio collector and input the analog signal to the IN1_L and IN1_R pins of the 3204. We want to know the correspondence between the acquired analog signals and the digital signals. What is the encoding protocol of the 3204, please attach An example is given.
3.In the last experiment, our signal was from the acquisition interface to the input pins IN1_L and IN1_R of the 3204, and then from the DOUT of the 3204 to the C5517. The C5517 processed the signal and sent it to the DIN of the 3204, and then the HPL of the 3204 to the external device. We measured the output signal to find its positive and negative clipping. We guess the reason for the 3204 input voltage and output voltage limiting. Is the input voltage range of the 3204 chip 0-0.9? Please give a possible reason for this phenomenon. Please see Figure 2.
4. As can be seen from the picture of the previous question, the input signal and the output signal have a large delay, and some of the delay must be caused by 3204. What is the total delay of 3204? Please see Figure 2.
5. When using the C5517 evaluation board the day before yesterday, we connected an active speaker to the signal output connector of the evaluation board, which is connected to the HPL/HPR pin in the 3204. The speaker has a strange sound. After a short while, it is found that the 3204 can't capture the audio signal, and the IN1_L/IN1_R pin has no signal input. But occasionally, the 3204 can receive some signals, but the noise is particularly loud. We suspect that it may be a breakdown. Can you help explain the reason?
6. When using the C5517 evaluation board the day before yesterday, we connected an active speaker to the signal output connector of the evaluation board, which is connected to the HPL/HPR pin in the 3204. The speaker has a strange sound. After a short while, it is found that the 3204 can't capture the audio signal, and the IN1_L/IN1_R pin has no signal input. But occasionally, the 3204 can receive some signals, but only noise. And the 3204 HPL/HPR pin detected a voltage of 3.52V. Can you help explain the reason? Is the 3204 chip broken?