This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1864: For application of PCM1864 EVM

Part Number: PCM1864
Other Parts Discussed in Thread: , PCM9211

Hi team,

I've received the following questions regarding PCM1864EVM. Can you please answer the questions?

Configuration : 1KHz (1WATT) SINE WAVE input -> PCM1864EVM -> SPDIF output  -> to AMP

-. Can PCM1864EVM support the configuration?

-. Is the analog input a BALANCE type?

-. Is it okay to use coaxial cable for SPDIF output?

Thanks,

Sam Lee

  • Hi Sam,

    PCM186x EVM can support this configuration. If you want to run the PCM1864 as MASTER, I would recommend configuring the EVM in Mode 1 using PPC2 GUI. Below is the screenshot of how the configuration works...PCM9211 is used to convert I2S output to S/PDIF but we only support optical connector on the EVM.

    PCM186x can be configured for both SE or Differential Inputs using the PPC2 GUI or configuring the registers.

    Thanks & Best regards,

    Ravi

  • Hi Ravi,

    Thank you for your answer. I ask one more question.

    To use a coaxial cable, is it okay if they try to connect the wires to the pad of output optical connector after stripping the coaxial cable?

    Thanks,
    Sam Lee
  • Hi team,

    Can you please answer avobe question? If it's not available, can you recommend any way to transmit SPDIF output using a coaxial cable?

    Thanks,
    Sam Lee
  • Sam,

    You should be able to get this working w the above approach. You can take the SPDIF_OUT from PCM9211 on the EVM and connect to coax cable for your application. Thanks.


    Best regards,
    Ravi

  • Ravi, this EVM comes with something called the USB-I2X -- what is this, exactly?
  • Hi Andy,

    The USB to I2X board is board that gets shipped with PCM186x and the EVM can be controlled though the use of the USB using the included USB-I2X board. The USB-I2X board has following functions -

    • connects to a PC via USB and provides digital control signals to the EVM board via I2C
    • provide serial digital audio in and out from the PC to the EVM through an I2S interface
    • supplies all of the power required for the EVM through USB

    Did you order an EVM and not receive the USB-I2X board? if you are designing your own board, you will have your host processor to configure the part w all the required I2C writes and you will not need the same...

    Hope this clarifies your question. Thanks.

    Best regards,
    Ravi

  • Hi, Ravi,

    I didn't order an EVM. I happened to see this thread and saw that the EVM included this USB-to-I2X board and thought that such a little board is ideal for my own test use. I mean, if it was $20 it's a no-brainer.

    I also wondered what parts it used and whether source code for it was available.

    Thanks!