This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3262: Can I use CodecControl to directly achieve a simple function based on a script exported from PurePath Studio?

Part Number: TLV320AIC3262


Hi Team,

My customer checked with me if they can use CodecControl to directly achieve a simple function based on a script exported from PurePath Studio? if not, please kindly suggest a solution.thanks.

The chip is TLV320AIC3262.

The script from PPS is as below:

The codec control tool is as below:

  • Hi, Yue,

    If the intention is to run the code within the Codec Control GUI (CC),  it can be done by loading and executing the code in the Command window, accessible from the View button in the toolbar. If the intention is to configure the SAR ADC with CC, it is possible by using the SAR configuration window, which is accessible as well from he View button.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer