Other Parts Discussed in Thread: TPA2028D1
Hello everyone,
I have the problem with TPA2028D1EVM. I generate audio signal from my MCU DAC, and I checked whether there was a signal on the DAC output. When I connect DAC output with TPA2028D1EVM input pin, my signal fall down to 0V. Register configuration on amplifier are: 0xC3, 0x05, 0x0B, 0x00, 0x06, 0x3A, 0xC2. I generated this configuration with the TPA2028D1 Interface software. There is no error at I2C bus.
The picture below shows the connection of TPA2028D1EVM:
(1) Green cable is DAC output
(2) Yellow cable is VDD from my power supply
(3) Brown cable is GND from Power supply
USB_PWR jumper is removed, because I use external power supply. I checked PVDD and it is on 5V. Do you have any idea what the problem is?
Thank you in advance,
Nikola