This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3140D2: Asking fort the possible solution to support 16ohm 12V to 5Watt

Part Number: TPA3140D2



Hi team,
Customer uses the TPA3144 and cannot meet 5Watt output at 12V/16ohm.
Can TPA3140 aceieve this output power? or it is the PVDD constrain?
If increasing the PVDD, can the issues be fixed?

This is the TPA3144 THD @ 12V/16ohm case.

e2e.ti.com/.../711366

BR,
SHH