Part Number: TAS2557EVM
Other Parts Discussed in Thread: TAS2557
Hi,
How to download the Pure Path console 3 for TAS2557EVM?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS2557EVM
Other Parts Discussed in Thread: TAS2557
Hi,
How to download the Pure Path console 3 for TAS2557EVM?
Yea
I got PP3 console however there is a problem
By checking HW I have had messages as
Unable to playback from device A
Unable to playback from device B
PC re-booting, board changing and re-plug USA connection all do not help.
The playback is OK but symptom like there is no EQ control.
Unable to playback audio from Device A
Unable to playback audio from Device B
Ivan,
Unfortunately due to LGE security policy I cannot attach any screenshots. Furthermore I cannot follow your links in e-mail.
The steps are standard:
1. Connect USB cable
2. Turn on Power 5 VDC
3. Start PP3
4. System check and follow the instructions
Download successful to Device A
Download successful to Device B
Hardware ID is good
Audio sound card detected and unambiguous
Audio sound card sampling frequency is good
Unable to playback audio from Device A
Unable to playback audio from Device B
Ivan,
Thank you for your feedback and proposal.
I checked with volume max 18 dB setting but problem still as before.
The calibration tone audible from both channels without any distortions.
But by changing EQ setting timbre does not change which means EQ does not work.
Ivan,
Thanks this resolve the problem.
Another issue whenever I apply EQ settings the timbre of the sound does not change.
Seems to me the EQ does not take any effects.
Do you have any hints to resolve the issue?