Dear all
There is a 49.9KΩ resistance in the INP and INM interface,below schematic, what is the function of the resistance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all
There is a 49.9KΩ resistance in the INP and INM interface,below schematic, what is the function of the resistance.
The 49.9kOhm resistors are to bias the input coupling capacitors. Since we do not know the source that will be driving the EVM, we must provide a method to keep the input connector at 0Vdc for the unknown source. In the final system design these resistors may not be needed.