This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3221: gain settings

Part Number: TPA3221


Hi all,

the TPA3221 gain can be set to 18dB, 24dB, 30dB, 34dB choosing the proper values of R1 and R2. My question is: does it possibile to increase the gain more then 34dB (for example 40dB), changing the value of those resistors?
Thanks in advance,

Nicola

  • Hi Nicola,
    TPA3221 supports four-step selectable gain settings, and they are fixed inside the AMP device. Any other gain setting is not supported. You could adapt the input analog signal amplitude to achieve the appropriate output signal.
    Best regards,
    Shawn Zheng