This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Currently, I amusing the power amplifier (LM1875T) that your company sells.
I am trying to amplify the amplitude by about 1.2 times by making inverting amplifier circuit using LM1875T.
We set the waveform which multiplied the signal of 200 Hz and 40 kHz to the input signal to the power amplifier.
However, when observing the waveform output from the LM1875T with an oscilloscope, it is observed that the amplification and extinction of the waveform are alternately repeated
Also, similar phenomena occurred when observed with the A / D converter, and it was also observed that the amplitude was shaken off at the moment when the waveform switched from the amplified state to the disappearing state.
As the picture shows how the waveform is amplified and disappears, you can show it if necessary.
Is there any cause for such a phenomenon?
Thank you.
Hello Mr.Shawn Zheng
Thank you very much for your reply.
I show you SCH and A photograph of the input voltage and the output voltage observed at the same time using the A / D converter.
I set the input voltage to about 4 V and I want to set the output voltage to 4.8V.
As I mentioned earlier, output waveform repeats amplification and extinction.
In the pictures of the waveform, The yellow waveform is the output voltage and the red waveform is the input voltage.
First picture is SCH.
Second picture is just before the amplified wave form appears.
Third picture is just before the amplified wave form appears(zoom version).
4th picture is just before the amplified wave form disappears.
Last picture is just before the amplified wave form disappears(zoom version).
Best regards.
Hello,
To refer to your advice, I attached heat sinks to the power amplifier(LM1875t).
I was able to amplify the output wave form.
Thank you very much.
Ukita Yuki