Other Parts Discussed in Thread: PCM4222, , PCM4202
References:
PCM4222 SBAS399A, page 4: PCM output, quad speed, fs = 192khz unweighted 22Hz to 40KHz
PCM4204 SBAS327A, page 4: PCM output, quad speed, fs = 192khz unweighted 20Hz to 40KHz
I noticed that the DR of the PCM4222 at the above settings is 118dB and the PCM4204 is 108.
is the 4204 DR a typo? What is the explanation for the 4204 value of 110dB
It seems like the 4204 would have the same/similar guts as the 4222
What are the unweighted DR values for the 4204 48KHz and 96KHz rates?
BTW, the 4202 at the same settings and rates is 117dB
Thanks,
Ed