Hi Experts,
is it possible to use the PCM186x for sensing wheatstone bridges ?
The part offers good ADC, fast sampling and valuable filtering options, that would make it attractive to use.
Well a wheatstone bridge type of pressure sensor is not a real microphone...
However, it´s also not too far of it. It has a bias of half of power supply (VDD=3.3V). The signal is differential.
Signals of interest are in range 1Hz till 10kHz. So I wonder if it works with PCM186x ?!
Any advise how to connect and setup in PurePath? (Currently try to use "differential input" on Ch1 right with 2P - 2M, Gain0)
Is there a code part (C-code) available for reading out the ADC values by I2C ?
and/or
How can the PurePath console help in case by using the direct I2C Read/Write function ?
Thanks,
Stefan