Hi there,
Can you kindly tell me what are the differences between these two parts?
Part: a). TAS5424ATDKDRMQ1 b). TAS5424ATDKDRQ1
Thanks and Best Regards,
Philip
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Philip,
We are looking into this, and will get back to you next week.
This week is a holiday in the US.
-d2
Philip,
The part numbers differ by the letter "M". The "M" indicates that the device has been through a monitored burn in.
Philip,
“Monitored burn-in” means that the parts are actually being verified during the burn-in process. So we set the devices to 22V in a 125C oven and start switching the outputs. We then monitor the health of every device during the process through test scan patterns.