Other Parts Discussed in Thread: TAS5086, TAS5631, TAS5162
Hi,
We succesfully developed several pro-audio products incorporating the TAS5086
in combination with TAS4062 or 5631 bridges. These bridges run at 384KHz at an input rate of
48K samples. We are happy with the specs and performance sofar.
However, for a very specific application, I need a PWM switching rate of approx. 190K, half
the original frequency. The tas5086 is driven directly from a 6713dsp MCASP, so reducing samplerate
is not a problem. Undoubtly, the internal PLL of the modulator has to run on this lower frequency as well.
Is this possible with the TAS5086? How should this be accomplished?
kind regards
Geert de Vries
Duran Audio BV