The TAS5731M datasheet describes the ADR/FAULT pin as "dio", digital input / output. But this same description is also used for the SDA pin, which is typically open-drain (standard I2C). However, in section 7.6 of the datasheet, both ADR/FAULT and SDA have a definition for "high-level output voltage", which does not seem consistent with an open-drain output.
Is the ADR/FAULT pin push-pull or open-drain when configured as the FAULT output? We are designing a system that will use two TAS5731M amplifiers, and if we can just strap ADR/FAULT low for one and high for the other (through 15k resistors, as described in the datasheet) and still be able to use the FAULT output, we're good to go. But if we need some additional circuitry because it is an open-drain output (like SDA, which has the same specifications in the datasheet), we want to be sure to add that before the PCB goes out.
Thank you!
-Dan