This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1739: TJ specification

Part Number: PCM1739


Dear Technical Support Team,

I have a question about PCM1739E/2K. 

Could you tell me the spec of Tj?

Best Regards,

ttd

  • Hi ttd,

    We do not have a specification for TJ on this device, but we did specify a maximum operating temperature in the Absolute Max Table of 70°C. If you use the TJΘ to estimate the ambient to junction temperature. If they device dissipates 93 mW (typically) and has a TJΘ of 100°C/W, then the junction to ambient temperature is about 9.3°C.

    Thanks,
    Paul