Other Parts Discussed in Thread: TAS5602
Hi,
We have designed a board utilizing three TAS5602 chips. Problem is, the amplifiers have a very high background noise.
Some info:
We use the stages in BTL mode
Decoupling is better than in the reference design
We don't have a real output filter, we only have ferrite beads and followed by a small capacitor to GND. The noise does not disappear if we mount a proper output filter.
The PWM lines feeding the amps are about 8 cm long, potential problem?
The amount of noise differs between the channels. But each of the three chips have one "good" and one "really bad" channel. If we connect the PWM signal from a good channel to a bad one, the bad channel is still noisy, so it's probably not the PWM that is bad.
The 24V line, the one powering the chips, seems OK when measured with oscilloscope, same for 3.3V.
A FPGA generates the PWM
The noise is mostly white
Anyone have any ideas or tips?
//Chris