This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5733L: Low power mode with PVDD in shutdown

Expert 4850 points
Part Number: TAS5733L


Dear e2e support,

To minimize the power consumption of our IC, are we allowed to shutdown the supply on PVDD (just keeping AVDD/DVDD)?

If yes, what would be the minimum expected quiescent current on AVDD/DVDD, in this case?

In any case, is it possible to be under a very low power mode, with the I2S bus that continues to work properly (as MCLK, SCLK, LRCLK, SDIN are used by other I2S devices in the application)?

Regards,

  • Hi Sebastien,
    The AVDD/DVDD current is around 49mA in normal mode, and it decreases to ~23mA when driving RST to low.
    Best regards,
    Shawn Zheng
  • Hi Shawn,

    Thanks for your feedback.

    My question was more related to PVDD:

    1- are we allowed to shutdown PVDD (I mean not provide any supply on it)?

    2- on that case, should we expect the same quiescent current on AVDD/DVDD as if we are in RESET?

    3- what would be the consequences on the I2S bus? Does it continue to work properly?

    Regards,

  • Hi Sebastien,
    See my answers below:
    Q1: PVDD is allowed to shut down, please let AMP enter shutdown mode(by writing register)
    Q2: No, the current consumption on AVDD/DVDD is lower with RST in low voltage.
    Q3: Digital part still works after configuration. When PVDD is applied and AMP exits shutdown mode, the output is recovered.
    You could try this on the TAS5733L EVM.
    Best regards,
    Shawn Zheng