Part Number: TAS5805M
Other Parts Discussed in Thread: TAS5805
Hi sir
The exported .h file is too large, could you help check whether delete the initial value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Darren,
Generally speaking, the length of .h file is related to how many features are activated.
For example, one biquad needs 5 * 32 bits initialization script, so the length of both left / right 15 biquads are 20 * 5 * 32 bits.
Anyway, PPC3 also support to generate only active components at the setting button. You can try to disable the default features.
Rdgs,
Matthew
Hi Matthew
now we have writed the code into the platform, however, we find that the code donot work, which cannot play sound. Just analyzed, through the software write address into it, 5805 did not answer. could you help give some suggestion how to dubug it,tks!