Part Number: TLV320DAC3203
Other Parts Discussed in Thread: TLV320AIC3254
Hello.
We chose TLV320DAC3203 for high-resolution applications (24bit-96KHz sample rate, need good frequency response at 20~40Khz) but encountered some problems on EVM.
The EVM Line in input capacitor reference is recommended to be placed at 0.1uF, and the frequency response is very poor (-3dB points are more than 200HZ).
Changed to 1uF, the situation improved, but still not good enough, we hope that the target is at least -3dB point at 20HZ, currently added to 4.4uF, there is also 5dB attenuation at 20Hz.
Normally, the audio codec line in should have high impedance (the actual measured EVM input impedance is close to 70K ohm), Theoretically the input capacitor should not need to be added to such to high.
Please help suggest if there is a better way to Improve results.
In addition, the output capacitor EVM is 47uF, we increase it to 220uF, the BT I2S output low frequency response is not OK, and later adjusted to 440uF is closer to our demand,
but the 440uF MLCC capacitor is very large and very expensive (we can not consider Solid capacitor),
If need to put such a large capacitor, the price advantage of this codec no longer exists...
Is it necessary to replace the codec with cap free? Thanks for kindly help~