Part Number: TAS5825M
Dear Ladies and Gentlemen,
we are planning to use a TAS5825M for our future product line. We don't want to use an EEPROM connected to the Amp, but instead have a large Flash connected to an FPGA. The FPGA is supposed to load the configuration from the Flash and send it to the Amp via I2C. Now, I already generated a .eeprom and .cfg file using the PPC3 software. Unfortunately these files are not binary. How can I convert the .cfg files to the binary format? I would really like to avoid to implement a script decoder in hardware. Thank you very much in advance.
Sincerely,
M. Werner