Hi
Do you have the voltage waveform of SPKP and SPKM and the current waveform of SPEAKER when TAS2505-Q1 plays sound for our reference?
Thank you
Jerry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Do you have the voltage waveform of SPKP and SPKM and the current waveform of SPEAKER when TAS2505-Q1 plays sound for our reference?
Thank you
Jerry
Hi, Jerry,
I took some captures of the voltage waveforms at the SPK outputs of the TAS2505-Q1. The TAS2505-Q1 is configured with a speaker driver gain of 12dB. I used a 1-kHz full-scale digital sine wave signal and 48KHz sampling rate. Yellow waveform is the SPKP output and Blue waveform is the SPKM output. Red waveform is the difference between both signals. This was directly measured on a 4ohms speaker load.
Then, if the outputs are filtered with an LC-filer, the outputs became clearer and easier to analyze.
Regarding the current waveforms, it is important to mention that the current will vary from speaker to speaker. Each speaker load has its own characteristics. However, in general all the current waveforms follow some forms depending of how much voltage is applied. Please take a look at picture below for details:
I hope this helps. Please let me know if you require additional information.
Best regards,
Luis Fernando Rodríguez S.