In our project we are planning to use 8 pcs of TLV320AIC3268, with each working upon a stereo audio signal (in1L & in1R ->ADC ->DSP ->DAC -> LOL&LOR)
each of the devices can output I2S lane. Is it possible each device to receive an I2S or TDM lane on one of the Audio Signal Serial Bus and to output a TDM on another Audio Signal Data Bus while including the channels of its own ADCs? The idea is to have at the last device a TDM output with all the channels included and minimal delay. We can accept to include either one (preferably two) audio channels per device until at the end we have 8CH (preferably16CH) entering in a microprocessor for further processing.